Other Parts Discussed in Thread: LM5022, , LM5118, TINA-TI
Hello Team,
We want to use the LMP8646 to use the LM5022 as a CC and CV source.We needed some help in reviewing our design. The design is current limit of 2A. Output voltage from LM5022 is 54.6V. We got the
output accuracy as 5.55%, Gain resistor 56.8K but approximated to 58K, is this ok?
Output resistor requires the minimum voltage (VO_REG_MIN),how do we find this for our application,or do we put the default 50 ohm?
We have taken BW recommended in datasheet 1.75K
and sense resistor as 55m ohm
A review on this would help us a lot
Thanks