Part Number: LM124AQML
Hello,
concerning the LM124AWRLQMLV, it is available per SMD with 2 variants:
- High Dose Rate: 5962R9950401VDA
- Low Dose Rate: 5962R9950402VDA
I read in the SMD that:
"The manufacturer supplying RHA parts on this drawing has completed Lot Acceptance testing at Low Dose Rate
(10 mrad/s) on these RHA marked parts. The Low Does Rate (LDR) testing that was performed demonstrates that these parts from the lot tested do not have an Enhanced Low Dose rate Sensitivity as defined by Method 1019, condition D. Lot Acceptance Testing at LDR will continue to be performed on each wafer or wafer lot until characterization testing has been performed in accordance with Method 1019 of MIL-STD-883. Since the redesigned part did not demonstrate ELDRS per Method 1019 and the previously tested device was ELDRS, the part number will be changed to an 02 device to distinguish the two parts. "
What is the status now?
Can I consider that variant 01 (High Dose Rate) is also considered as ELDRS free?
Or, at least, is there a minimum date code from which I can be sure that both variant are of the same die design, and thus, ar both ELDRS free?
I thank you very much in advance for your support
Guillaume