Part Number: TLV7022
Other Parts Discussed in Thread: TINA-TI
I am supporting an application using the TLV7022.
The application has seen some concerning behavior during system-level noise testing.
As we work through figuring this out, I need the following info.
1. What is the response time to a pulse of the TLV7022?
how wide does the pulse width have to be in order for the TLV7022 to respond?
2. Is there a parameter in the datasheet for this? Which parameter(s)?
3. Is there a comparator that won't respond to really short pulses (short being maybe IEC61000-4-x burst pulses)? Hopefully P2P?
The current application uses TLV7022 with <410kHz input signal.
Is there a solution/device that won't respond to pulses shorter than 2.4[us]?
Regards,
Darren