Okay, I have the following case:

Board 1 is a backplane board and has some (multiple) insertable boards in the shape of board 2. Board 2 has local power supplies that we don't want to cross over to board 1 due to various reasons. Now what we want to do instead is have a weaker pull resistor that is always placed and then depending on the address that is desired one of the 3 optional resistors can be placed on board 1. Now my question is this possible for the 0R to SDA or SCL? What would be resistor values that work?
Thanks in advance!