Other Parts Discussed in Thread: BQSTUDIO, , BQ25895M
I have a HPA665-001. USB2any using the BQSTUDIO v1.3.101.
I am trying to configure BQ25895MEVM evaluation module. I am not able to see the USB2any but when I open the usb2any explorer program it says I need to update the firmware.
I have unplugged the usb2any, held down the switch and plugged the unit in and it comes up saying to update the firmware. If I click update, it does properly update the firmware and the LED stays solid.
As soon as I close the explorer program the led starts to flash. If I reopen usb2any explorer, the led will go steady again.
If I open battery management studio it says "no free adapters are available for use on this system. Near the top it says "device ACK error"