Hello
I have a question about mpy634 frequency range.
Can I use MPY634 about frequency range 1.6Khz~0.1Hz?
If not, Can you recommend another IC chip?
Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
I have a question about mpy634 frequency range.
Can I use MPY634 about frequency range 1.6Khz~0.1Hz?
If not, Can you recommend another IC chip?
Thank you.
There is no minimum frequency. You can extrapolate from the typical performance curves.
Please note that using an analog multiplier is quite unusual nowadays. Wikipedia says:
In most cases, the functions performed by an analog multiplier may be performed better and at lower cost using digital signal processing techniques. At low frequencies, a digital solution is cheaper and more effective and allows the circuit function to be modified in firmware. As frequencies rise, the cost of implementing digital solutions increases much more steeply than for analog solutions. As digital technology advances, the use of analog multipliers tends to be ever more marginalized towards higher-frequency circuits or very specialized applications.
In addition, most signals are now destined to become digitized sooner or later in the signal path, and if at all possible the functions that would require a multiplier tend to be moved to the digital side. For example, in early digital multimeters, true RMS functions were provided by external analog multiplier circuits. Nowadays (with the exception of high-frequency measurements) the tendency is to increase the sampling rate of the ADC in order to digitize the input signal allowing RMS and a whole range of other functions to be carried out by a digital processor. However, blindly digitizing the signal as early in the signal path as possible costs unreasonable amounts of power due to the need for high-speed ADCs. A much more efficient solution involves analog preprocessing to condition the signal and reduce its bandwidth so that energy is spent to digitize only the bandwidth that contains useful information.
In addition, digitally controlled resistors allow microcontrollers to implement many functions such as tone control and AGC without having to process the digitized signal directly.
Please tell us what is the actual problem that you're trying to solve.
Hi Hoonmin,
yes, you can use the MPY634 down to 0.1Hz. But you may see an increased noise level at very low frequencies.
Do you still want to use the MPY634 in a mixer, according to this thread?
Can you tell more about your application?
Kai
Thank you about your reply.
Yes I want to use the MPY634 in a mixer like that thread.
I want to make Lock in amplifier using MPY634 for calculating LIB(Lithium Ion Battery) impedance
LIB impedance magnitude is very small(mohm) and we want to calculate 1.6Khz ~ 0.1Hz range of LIB impedance.
Thank you !
Hi Hoonmin,
in a lock-in amplifier the "multiplier" is usually implemented by the help of a "synchronous demodulator" forming a "phase sensitive detector":

See also this link:
https://experimentationlab.berkeley.edu/node/99
Kai
Hi Hoonmin,
Yes, I will confirm that the MPY634 can be used at this frequency range. It can be used from DC up to the frequencies specified in the datasheet.