Part Number: OPA548
Other Parts Discussed in Thread: OPA547
Hello,
I am a novice in these matters, so I apologize for any incomplete or incorrect explanations.
I have a 10 V-20 mA signal generator. I can adjust the frequency and amplitude.
I want to drive the BLDC motor the way I want. Of course the current is insufficient.
Operating voltage range: 12-24V
Idle current: 55mA
Power 7.5W
I have examined many amplifier circuits but I could not find a circuit I wanted.
Will the OPA548 integration help me?
If you have a different suggestion, could you share it with me?
Thank you in advance.