Part Number: OPA656
Hello.
I have designed in the OPA656N amplifier and am quite pleased with the performance. Except for the excessive heat generated by the part. We are entering production and I am under a great deal of pressure to get this solved. Package is SOT-23-5
1) Amplifier is a unity gain summation amplifier, (see schematic).
2) Solid ground plane underneath the footprint, (see layout).
3) Power supplies are from LDO which are very clean.
4) All components are close to the associated pins, (see layout).
5) Measured current is approximately 15ma per power pin. Total power is 150mw.
6) Output is stable with no oscillations.
Measured temperature at top of component is 50 degrees Celsius with a room temperature of 21 degrees Celsius.
I do not understand why this device is running so hot.
I have been designing with T.I. parts since 1978 and here's hoping your team can solve this one.
This is a great amplifier with low bias current, and low output offset. The only issue is the heat.
We are getting ready for production and have to solve this ASAP.
Attached are the clips of the schematic and layout.


I look forward to a quick response,
Thanks,
J. Allan Jarvo
Principal Hardware Developer
Email: jarvo@kwesst.com
Cell: 613 293-3096
KWESST Micro Systems Inc.
Canadian Head Office:
155 Terence Matthews Cr.
Ottawa, ON. K2M 2A8
www.kwesst.com TSXV: KWE
This message and/or attachments may include information subject to KWESST Corporate Policies and is intended to be accessed only by authorized recipients. Use, storage and transmission are governed by KWESST and its policies. Contractual restrictions apply to third parties. Recipients should refer to the policies or contract to determine proper handling. Unauthorized review, use, disclosure or distribution is prohibited. If you are not an intended recipient, please contact the sender and destroy all copies of the original message.