Hi TI team,
We are using INA220 current sensor circuit in our design and the circuit is as shown below. It has been observed that there is 100mA to 200mA difference between the measured value and applied load current.(Higher the load, larger the difference in measured current value).
INA220 Circuit:

Measured current values:
| Applied load | Current sensor Measured value |
| 300mA | 410mA |
| 400mA | 520mA |
| 500mA | 645mA |
| 600mA | 775mA |
| 700mA | 885mA |
| 1000mA | 1200mA |
| 5000mA | 5999mA |
Register Configuration is set as per datasheet (Since our circuit is same as Figure 30 of datasheet):

Can you please support us on resolving the same?
Regards,
Vidhya