Other Parts Discussed in Thread: OPA2677
Hi Team,
Please advise on the following question.
I consider to use THS3491 in a system which requires stringent HD2 and HD3 performance.
The THS3491 datasheet insists HD2 and HD3: Less Than –75 dBc (50 MHz, VO =10 VPP, 100-Ω Load)
It is also stated HD2 -78dBc (typ)@f=20MHz in the Electrical Characteristics table.
I want/need to know how much the HD2, HD3 validated depending on the lot validation.
Q1. Don’t you have any data on the HD2/HD3 validation?
Q2. If so, can you share the distribution profile (es: Gaussian or other curve) and its standard deviation?
Best Regards,
Nishie