Part Number: LMH6551
Other Parts Discussed in Thread: THS4561, TINA-TI, THS4541, LMH6550, THP210, THS4120
Hello:
There are sooo many options for selecting a suitable opamp for our application!
Pl see screenshot of the circuit using LMH6551.
Although we won't scan below 100Hz, the input signal comes from a network analyzer sweeping up to 10 MegHz.
We had to generate -5V in our system circuit just to address CMR issue. The output needs to be with very low CM - because the channels are connected to the same Network analyzer which may not support much DC.
Is our selection and circuit "correct" in view of the application needs?
BTW: output has very large value capacitors- hopefully of equal values- to isolate common mode DC at the capacitor nodes- on the left side.
Any review will be highly appreciated.
-r