Other Parts Discussed in Thread: LM6171, LM7171
Hello E2E Experts,
Good day.
Thank you in advance.
I have been searching for an amplifier for my setup and I was told that an operational amplifier is what I'm looking for.
I need the amplifier to amply pulses up to ~25-30V with a pulse length of 200nm to 1ms.
The lower pulse length limit is a must while the upper limit is not.
I think you would also need to know that my output has a maximum voltage of 5V DC. I would need the pulse amplified to have a 20V ppV, which is a square pulse from 0-20V and not -10-20V
Regards,
CSC