Part Number: LM741
Other Parts Discussed in Thread: LF356, TL071
I am using the attached circuit.
It is a standard inverting amplifier circuit.
There is a class D switching amplifier nearby and the switching frequency is 51 kHz.
Noise from the switching amplifier seems to be on the input and output of the LM741.
The supply voltage is ±15V.
The input voltage is ±50mV to ±200mV and the frequency is 40 to 55Hz.
When the output of the switching amp is turned up, the negative output of the LM741 is inverted.
This is an unintended behavior.
If I replace it with an LF356 or TL071 with the same pin assignment in the same circuit, the output is normal.
This is strange.
My questions are
(1) Are there any possible causes?
(2) Is there any difference between the LM741 and the LF356/TL071 with respect to high frequency noise?
I would appreciate it if you could answer my questions.