Part Number: INA2132
I am looking for the junction-to-case and junction-to-board thermal resistance for the part: INA2132UA.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: INA2132
I am looking for the junction-to-case and junction-to-board thermal resistance for the part: INA2132UA.
The junction-to-case and junction-to-board thermal resistance is specified only for IC packages with thermal pads. Since INA2132UA uses a standard SO-14 package with no thermal pad, only a junction-to-ambient thermal resistance is specified - see below.

In a conduction cooled system, with negligible convection to the environment, what is the recommended calculation for the temperature then?
My conduction cooled model will have the board temperature, but not an easy way to estimate the ambient temperature since the system is enclosed and subject to a range of environments.
Claudia,
Even if we could provide you with junction-to-case thermal resistance for INA2132, a board temperature is not equal to the case temperature in the packages with no thermal pad. My advice would be to try to use a temp sensor to measure ambient temperature inside the system enclosure, which may be easier said than done.
As I mentioned, the system is conduction cooled. So the PWB would also be cooled via conduction.
Below please find INA2132 reliability data including including MTBF of 4.71*10^9 at typical Usage (junction) temperature of 55C.
https://www.ti.com/quality/docs/estimator.tsp?opn=INA2132UA&cpn=&partNumber=INA2132#resultstable

The equivalent MTBF for different usage temperature may be calculated using Acceleration Factor based on Arrhenius Equation:

For example: