Other Parts Discussed in Thread: INA296A, INA281-Q1, INA240-Q1, INA241A, INA293-Q1, INA190-Q1
Hi Expert,
May you kindly suggest one device with similar spec but higher CMRR than INA181-Q1? And they are pin compatible.
Thanks!
Ethan Wen
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hey Ethan,
There really is no pin-to-pin compatible device with the INA181-Q1 (SOT23-6). The closest device is INA281-Q1/INA293-Q1, but this device is not bidirectional and thus does not have a REF pin, which could be critical to the design. Bidirectional devices with better CMRR and similar functionality are INA296A/INA241A (no automotive qualified version... yet), INA190-Q1, and INA240-Q1.
Here is a broad parametric search using key filters (>25V Vcm rating, SOT23/SOT23-thin, bidirectional):
Sincerely,
Peter