Other Parts Discussed in Thread: INA138, INA139, INA183, INA241B, INA296B
Hi team,
My customer is looking for the high side current sense amplifier which meets below requirements. Do we have such a device?
Purpose: Sensing current for OCP
Vcc max: over 15V
minimum operating power supply voltage: above 5V
Analog inut(IN+) and Analog input(IN-) should be over 10V.
Package: SOT-23 5pin or 6pin.
Low cost
Best regards,
Shunsuke Yamamoto