Part Number: TLE2426
The SPICE model for TLE2426 doesn't work with floating circuit simulations, see below. V+ should be 5V, and V- should be -5V. There should be NO CURRENT in the output of the '2426.
I compared this with an equivalent circuit built from TLV9102- this provides correct results, also shown below

The TLE2426 model is ancient, the one included in TINA appears to be the same as the latest in the product folder (just wrapped up for PSPICE). This bug has wasted a lot of time and very surprised this hasn't been revealed in the previous 25-30 years...
Please fix this, especially in light of the fact that this part will likely be updated with migration to RFAB (hopefully).
Attached simulation in case you would like to see it.
-Steve