The product description can be enlarged 20 times, but the actual amplification can only be 2 times. Please help to confirm the problem
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The product description can be enlarged 20 times, but the actual amplification can only be 2 times. Please help to confirm the problem
So I think your gain to the output pin is about 11V/V,
0.5Vpp will then be 5.5Vpp and at 400MHz, the slew rate demanded will be 2.25Vpeak*6.28*400MHz, =7000V/usec which exceeds the available 5500V/usec in the OPS,
Why don't you back off to 200MHz and see if the amplitude makes more sense.
Hello user,
Were you able to obtain the correct output at the lower frequency suggestion by Michael?
Thank you,
Sima