Part Number: INA186-Q1
Other Parts Discussed in Thread: INA186
Hi team,
From the functional safety purspective, I would like to know the maximum input to output delay of INA186A2-Q1.
I think the bandwidth of the device is 37kHz typical and the delay seems ns order, It should be around 30us(typ).
How much is the max tolerance of this delay?
Actually <1ms is more than enough, so <x10 variation is acceptable.
regards,