Hi
Follow up from this post: https://e2e.ti.com/support/amplifiers-group/amplifiers/f/amplifiers-forum/1063699/ths3491-amplifier-power-down-not-always-behaving
"We are using the THS3491 (RGT) package in our design with bipolar +/-14V rails. We use a single power down signal for a bank of THS3491 amplifiers to power-down all of them at once, with the power down either at 5V or 0V. We have observed on some boards that have been built one amplifier will appear to only partially shut-down, and appears to still draw the full quiescent current from one of the rails (i.e. the 14V OR -14V, but not both). The power-down line is measured to be 0V and the other amplifiers are fully shut-down, but the problematic part is only half shut-down and will generate a several volt offset voltage at the output."
We are still seeing this issue occurring on our production units, still several % showing the issue in each production run we do.
We have confirmed that when the THS3491 is failing to power down, there is either 0.2V present on the +IN and -IN pins, or 0V present on the input pins (depending where in the circuit the problematic part is). But it doesn't seem to matter what this voltage is. The PD pin is 0V when showing this issue, and the rails are present and stable at +/-14V.
Any ideas would be appreciated.
Thanks
Jordan