Part Number: TLV7044
Hi everyone.
I'm making a circuit that uses the TLV7044 chip.
I have a question about the propagation delay parameter.
The tlv7044 has a propagation delay of 3 usec.
If on the inputs of the comparator i had a differential pulse that lasts less than 3 usec, would it still propagate to the output?
For example, if the non-inverting input were fixed at +1volt (vref) and on the inverting input there was a direct voltage of 4V which goes to 0volt for only 500nsec
and then returns to 4V, I would be able to see the pulse in the output?
Best regards,
Luca.