Other Parts Discussed in Thread: LMH6612, OPA356, OPA836
The LHM6611 is supplied by +/-2.5V (as below circuit), when the device input is set from 0V to 1.0V, then the ouput of LHM6611 is saturation at 1.7V .
according to LHM6611 data sheet, it says "The amplifiers will operate on a 2.7V to 11V single supply or ±1.35V to ±5.5V split supply. ",
when the LHM6611 is supplied by +/-5.0V, when the device input is set from 0V to 1.0V, then the ouput of LHM6611 can reach at 2.0V which I expected, what is wrong for below circuit?