Hi Experts,
Seeking your assistance on this query from Cx:
They have two problems with LOG101.
- Output of LOG101 have ripple in the upper voltage decades.
- Output voltage amplitude shifts up and down on base input current.
Problem 1:
In first step they connected LOG101 as is notice in datasheet.
- Vcc = ±10V (20V)
- Cc = 47pF
- I1 = 10µA
- I2 = sawtooth amplitude0-10V / 1Mohm
- F_I2 = DC to 100Hz.
Noticed that LOG101 output had ripple in the upper voltage decades.
In second step they connected LOG101 as in Figure 1 below.
Noticed that its output had even bigger ripple in the upper voltage decades as before in first step. For that reason, they began to reason that the output LOG101 is overloaded and so did another experiment (follow step third).
Figure 1:

In third step they connected LOG101 as in Figure 2 below (with output buffer).
Noticed that LOG101 output had the same ripple in the upper voltage decades as before in first step. The problem is that the output is oscillating on upper voltage decades.
They have a theory that it is overloaded by a capacitor Cc that prevents oscillation in the lower decades.
The connection is not on the PCB, but with short wires, the shortest way. If the problem was induction, it would be most noticeable at low currents and not at high currents.
Figure 2:

Problem 2:
Output voltage amplitude shifts up and down on base input current.
If they use a symmetrical amplifier at the output of LOG101, the amplitude of the symmetrical amplifier reaches saturation in the lower or upper decade, because LOG101 shifts the output on base input current range.
In addition, the LOG101 does not have 8Vpp at the output as stated in the datasheet, but only something around 4V, which I am trying to amplify to +-10V. Their question is why does the amplitude move up or down?
For your assistance please.
Thank you.
Regards,
Archie A.