Part Number: OPA2695
Other Parts Discussed in Thread: OPA695
Hello,
I notice that the dual OPA2695 is covered by a different datasheet to the single OPA695, with the OPA695 looking to be considerably faster in terms of both small signal bandwidth and slew rate. I have an existing application that uses the 2695 but was wondering if I could extend the frequency range a little by changing to using 2 of the single parts instead so I had hoped to do a quick comparison in Spice. However, the model listed on the OPA2695 product page looks to be the single OPA695 model.
Normally I'd be happy to use the single model and take it to be representative of the dual part, as usually they have the same datasheet and essentially have the same spec. That doesn't seem to be the case here. Can you confirm which of the two parts the model is representative of and, if it's the single OPA695 as I expect, is there anything that can be done to model the dual part?
I'm also curious as to why the specs for single and dual parts are different for this one in the first place, as that's not usually the case.
Thanks,
Gordon.