Hi
We use the THS3491 in our production and have seen one instance out of several hundred where a THS3491 is fitted to a PCB, tested and working perfectly, then we package and ship the device somewhere else.
Our product uses 20 THS3491s, and in one instance we have had all 20 of the THS3491s working before shipping, then after the PCBA is shipped we see a single THS3491 fail. The failure in this case was an apparent short:
- With the THS3491 fitted on the board, the resistance from VCC and VEE to ground was ~50 Ohms
- With the problematic THS3491 removed from the PCBA, we see ~1 Ohm resistance between VCC and VEE, compared to ~Megaohms on a good part
I am looking for any suggestions of what type of fault could cause a working THS3491 to stop working in such a way. We tried to reflow the solder on the problematic THS3491, which made no difference. The solder pattern also looked fine after removing the part, with no obvious solder bridges.
Thanks
Jordan