Other Parts Discussed in Thread: MC33078, TLV9164, , TLV9364
Hi Team,
Is there any better suggestion to replace MC33079DR2G?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hey Kevin,
OPA4992 seems to be the best competitor to MC33079. Here is a comparison table. If cost is a concern, consider TLV9364, or if 30V supply is not needed, they could also cost-down to TLV9164.
► Part Number | OPA4992 | MC33079 |
Manufacturer | TI | ON |
Channel Count | 4 | 4 |
Vs Range | 2.7V to 40V | 10V to 30V |
GBW (MHz) | 10.6 | 16 |
Slew Rate (V/µs) | 32 | 7 |
Vos max @ 25oC (mV) | 1 | 2.5 |
Vos Drift, typ (µV/oC) | 0.25 | 2 |
Rail-to-Rail | In, Out | No |
IQ typ (mA) | 2.4 | 2.1 |
VN (nV/√Hz) | 7 | 4.5 |
ISC typ (mA) | 65 | 37 |
IBias (typ) (pA) | 10 | 300000 |
Operating Temperature (°C) | -40 to 125 | -40 to 105 |
Available Packages | SOIC-14, TSSOP-14 | SOIC |
Best,
Jerry