Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLE2022: alternative part

Part Number: TLE2022

Hello,
due to deliver challenges customers is looking for drop-in alternatives. Can he use TLE2022QDRQ1 or TLE2022AQDREP? Any differences?

Regards, Holger

  • Hi HS,

    The TLE2022Q-1 and TLE2022AQ-1 are the versions of the TLE2022 that are qualified for automotive in accordance with AEC-Q100. They also have an operating temperature range of -40°C to 125°C. The electrical characteristics of the Q1 and non-Q1 parts are essentially identical and can be a drop-in replacement within the operating temperature spec. Of course the A variant is slightly better in certain specs such as offset voltage.

    Thanks,

    Zach