Other Parts Discussed in Thread: LM293,
Hi There,
Please see attached image of LM293 used as comparator to monitor +24VDC supply. I am bit doubtful about the hysteresis provided as the reference is on inverting input. Can you please verify and provide your inputs to same.
Also diode D28 seems to be placed wrongly in circuit as at TP12 we are getting around 2.4V. It was placed to protect MCU pin from possible over voltages as opam is biased on 5V.
I want to use hysteresis on this existing circuit.
Thanks..!!!!