Part Number: THS4521
Other Parts Discussed in Thread: ADS1178, , THS4551
Hi TI Tech Team
I have an application interfacing a THS4521 to an ADS1178 16 Bit differential ADC. Vref of the ADC is 2.5V. Maximum input signal can be up to +/-15V sinusoidial,
which is why Ive opted to use the attenuation circuit suggested in SLYT341. Is there anything obviously wrong with my circuit? simulations seem OK to me, with
the input to the ADC being +/-2V (4V p-p). Any suggestions would be appreciated, ive provided Tina Simulations and a schematic below. Thanks in advance