The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

High Speed Photodiode Amplifier for ADC Drive

Other Parts Discussed in Thread: OPA857

We're designing an analog front end for a 5GHz bandwidth photodiode. We'd like to know more about TI products and strategies we could use to buffer the photodiode current to adequately drive a high speed ADC while maximizing bandwidth.

  • Hello Nicholas, 

      Thank you for your interest in our products! I have a few questions before I recommend devices/solutions especially due to your very fast bandwidth requirement. 

    1. Are you able to share the end equipment? We have two sets of transimpedance devices we recommend, our voltage/current feedback amplifier portfolio used as a TIA (transimpedance amplifier) or for a more specific GBPS optical communication, we have our ONET products which come as a die and typically used in optical networking solutions. 

    2. Do you need a wide gain range?

    3. Does your ADC require a differential input?

    4. What is your photodiode internal capacitance? 

    5. Any noise, supply configuration requirements?

    Best Regards,

    Sima 

  • Hi Nicholas,

    when it comes to stability and bandwidth the detector capacitance is the key factor here.

    Kai

  • We're planning to use the ThorLabs DET08CFC, Cj = 0.3pF in the datasheet. At these high speeds it seems most ADCs recommend if not require differential input, but we're evaluating how that impacts overall bandwidth as well. Right now we're reading up to 1.4V output into a 50 ohm load directly from the detector so I think 50 ohm transimpedance gain will be sufficient.

  • Hello Nicholas,

       Using this TIA calculator, system design requirements for 65 degree phase margin is below:

       Here is a link of filtered transimpedance amplifiers that are above the require GBP: If gain requirement increases; then I would suggest picking amplifiers with on the faster end for headroom. 

       Overall signal chain suggested below for TIA to differential signal conversion:

       We do have a TIA with pseudo-differential output if your design is space constrained which is the OPA857. Otherwise, a filtered FDA list can be found at this link.

    Thank you,
    Sima