Hello,
How to understand or read below mentioned line for Hysteresis
>>Hysteresis 0.2 volts around 7.62 volts.
Best Regards,
Kiranjit
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
How to understand or read below mentioned line for Hysteresis
>>Hysteresis 0.2 volts around 7.62 volts.
Best Regards,
Kiranjit
Thanks Clemens!!
Yes, it is not mentioned in datasheet but how did you calculated these two values?
Thanks,
Kiranjit
Hi Kiranjit,
Hysteresis essentially creates two dc threshold levels for the inputs to traverse through. If the hysteresis is a total of 0.2V, centered around 7.62V, then you VH level would be 7.62V + 0.1V = 7.72V and VL is 7.62 - 0.1V = 7.52V. Section 9.2 of the datasheet has an example.