Part Number: INA321
Hello,
I have been asked to review a scheme that uses the INA321EA.
The problem is that the output of the INA321 does not always have the same output voltage on different printen circuit boards in production. The component is used to measure the current flowing through R4 (100 ohm) (max 7uA) The circuit has been simulated in PSpice, but here I don't see the same result as in practice. (practice INA321EA max. output = 350mV)
Is it possible that a mistake has been made here, and that the Input Offset Voltage of the INA321 is not achieved.
Thank you for the assistance