Part Number: INA333
Other Parts Discussed in Thread: TL331, TLV3501
I'm simulating the INA333 in TINA TI. The amplifier will be sensing a wheatstone bridge.
My circuit generates a differential voltage of 0.06V. The expected output is:
+ ref
Where: ![]()
Gain = 1+ 100k/5.36k = 19.65
Therefore Vout = 19.65 * 0.06V + 1 = 2.179V.
The circuit includes a common noise filter at the input.
Additionally, R12 & R15 aim to keep the signal away from the supply rails.
Are there errors in my schematic?