This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team:
My customer want to use LM311 to capture 13V pulsed quadrature signal for MCU to detect high / low .
If the ref voltage for LM311 is 6.5V, does it work with single power supply 15V? The reason why customer choose LM311 is their Propagation delay time is low as 0.115us,or do we have another recommendation?
tks !
Here attached the customer waveform when we use LM2903:
blue one is 13V pulsed quadrature signal(<10Khz) ,yellow one is the square wave signal that MCU need. But too much spurs currently.
Hi Allen,
Thanks for reaching out. The input signal is a bit noisy so I would add some hysteresis to reduce the chatter that you are seeing on the output. Yes, LM311 would work with a 15V VCC single supply but just keep in mind that the input voltage range is limited to +0.5 to 13.5V. Are you using the balance and strobe pins? Do you need the ground shifted output? It would be helpful if you could show your schematic.
Hi Allen,
what shall be detected? Only the triangle wave? As Chi already suggested hysteresis has to be added. But the superimposed noise which can be seen on the left of scope plot is so high compared to the triangle wave's amplitude that the hysteresis must be set very high.
To suppress the superimposed noise and to ease the triggering of comparator some low pass filtering in front of the comparator may help.
Kai