This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA233: PAC1934T

Part Number: INA233
Other Parts Discussed in Thread: TIGER, INA3221

Hi

Could you help to suggest similar PAC1934T alternatives, Need to have 4senses

  • Gareth,

    We unfortunately do not have any 4 channel digital power monitors at this time. We have the INA32221 power monitor which is 3 channel, but the specifications are different than the PAC1934T. The closest cross we have here at the moment is the INA233, but it is only a single channel device. 

  • Hi Carolus

    The customer uses 2 pieces of PAC1934T to detect the 6 phase core power current on the Tiger lake platform Is the INA32221 suitable?

  • Gareth,

    There are some tradeoffs to the parts, but yes, 2x INA3221 could potentially work here. For example, the maximum bus on the INA3221 is 26V, where the PAC1934T can measure up to 32V. That may or may not be of concern to the customer. They will need to review the datasheet for the differences between the devices and ultimately decide if they will work for their use case.