Part Number: ISO124
Other Parts Discussed in Thread: ISO224, AMC1411, AMC3330
I need to take a continuous voltage measurement of approximately 60-260VDC, pass it across an isolation boundary of at least 1500V, and then create an analog representation of this voltage on the other side of the isolation boundary. I have a +15V rail available on the output side. I'm looking at using an isolation amplifier that allows me to utilize the full 15V at the output to hopefully increase the accuracy when scaling the voltage. Could I use this part to scale the input voltage between 0V and 15V on the output side?
Is there a different isolation amplifier that you would recommend or is there a different part that I should consider?