Part Number: INA186
Is it possible to reduce the input bias current of the INA186 using the following methods...
1. Disabling the device with the ENABLE pin ?
2. Switching off the power supply at the pin 1 (VS) (using an analog switch).
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: INA186
Is it possible to reduce the input bias current of the INA186 using the following methods...
1. Disabling the device with the ENABLE pin ?
2. Switching off the power supply at the pin 1 (VS) (using an analog switch).
Thanks.
Thank you Kai.
The Figure 6-7 is exactly what I was looking for but must have overlooked it.
So for my future reference...would the residual leakage when the device is disabled be due to INA186 input ESD protection ?
Also...would removing the power rail from the VS pin have any additional affect in reducing bias current any further ?
Thanks.
Hi Tony,
Glad you found figures 6&7 helpful (thank you Kai!). Regarding the other questions, I agree the residual would be mostly due to ESD cells. But the input circuitry likely can’t be completely cut off either.
I don’t think removing power supply will help with reducing Ib further.
Regards, Guang