This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM158-N: LM158-N-The high temperature test is abnormal

Part Number: LM158-N

The output and input of the test are relatively stable at normal temperature, but in the high temperature test, the temperature remains at 60℃, the input is stable, but the output fluctuation gap is relatively large. Please help check the cause