This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2903B-Q1: Unpowered Inputs

Part Number: LM2903B-Q1
Other Parts Discussed in Thread: LM2903B, LM2903, LM339

Hi - customer question below:

If 13.5V is applied through 49.9kOhms to the (+) input of a LM2903B that has no power applied to it (VCC=0V), is there any kind of positive-voltage clamping diode on that LM2903B (+) pin that would try to conduct some current to VCC? Or does that input not have any clamp on it for positive current?

Thanks!

Reed