Part Number: TRF37C75
Hello,
i did not find in the datasheet any information about the powerdown pin control dynamics, that is, the gain variation in dB between the device enabled and the device disabled through powerdown pin. So i'm asking if this measurement has ever been performed; i need it for setup of a PWM in a microwave power amplifier.
in the datasheet is reported that the powerdown logic levels are TTL but the minimum high input level is reported as 2V, which is compatible with 3.3 Volt logic. Traditionally the definition of TTL logic refers to 0-5V logic, so i'm asking confirmation that i can drive the powerdown pin with 0-3.3 V logic levels.
Best regards
Vasco