Other Parts Discussed in Thread: AMC1203
Hi Team,
My customer is evaluating AMC1302 with Tina simulation file below,
IL_sensor circuit_use AMC1302.TSC
there are some questions below from customer,
1. VM1 and VM2 are AMC1203 input and output waveform, there is some distortion with triangle waveform, is it due to AMC1302 BW limit?

2. the maximum input current is 80A with Rshunt 0.5mΩ
The output voltage should around 0.5mΩ x 41 x 0.845 + 1.5 = 2.8858V, but VF2 voltage is 2.76V. is there some loss in this circuit?
3. there is 1.54us output delay, is this AMC1302 internal delay?

Thanks & Regards
Eddie Chou