Part Number: OPA836
Other Parts Discussed in Thread: OPA838, , OPA837
Hi team,
My customer is using our OPA836 & OPA838 now.
And they wonder if we have a newer device to recommend.
Requirements:
BW: >200MHz
slew rate:>200V/us
Iq:<1mA
Thanks,
Brian
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Brian,
The OPA838 is still the best device to consider for this requirement. The OPA838 being a decompensated amplifier gives an excellent figure of merit with its very high 300 MHz GBW, 350V/us slew rate while consuming only 0.95 mA quiescent current.
Regards,
Bharat Agrawal