Part Number: ISO224
Other Parts Discussed in Thread: LOG114, ADS124S08
Hello,
I have to design an inexpensive (as much as possible) and simple (< BoM count) solution to measure leakage of semiconductors. The requirements are quite tough:
1- Measurement range 1nA to 10mA
2- Measurement over a shunt (alternative solution could be evaluated)
3- It has to be isolated, as the semiconductor connected in series to the shunt is in the >1.5kV class
4- Typically the shunt will not see high voltage, but we need to design it for short-circuit failures in the DUT and therefore we need an input protection of 2kV
What would you use?
Thanks