Other Parts Discussed in Thread: BUF802,
Hello!
I have purchased a BUF802RGTEVM to measure the bandwidth of the BUF802 chip. During the experiment, I used a signal source, an oscilloscope, two transmission lines, and BUF802RGTEVM. The signal source provides a sine signal with a power of 4dBm and a frequency set at 2GHz. The overall gain is -6.4dB. Then I used a network analyzer to measure the line loss of the two transmission lines. At 2GHz, the total line loss of the two lines is about -1.7dB, which means that the loss on the BUF802RGTEVM reaches -4.7dB. This clearly does not comply with the 3GHz bandwidth mentioned in the data manual. We hope you can provide some suggestions.
Thank you