Other Parts Discussed in Thread: THS4521, TINA-TI

In order to use the 16-bit mode of F28379D ADC, I would like to use 2 INA185 connected in reverse (VDD = 3V, output signals are biased to 1.5V) to create a differential signal to feed into ADCA4 and ADCA5 of the LAUNCHXL-28379D. Simulations show that this is possible but I would like to hear your comments on various potential scenarios that could affect this topology.
PS: I tried to use the fully differential THS4521 but the output signal is distorted near the rails and voltage offset at low signal level is not good compared to the above circuit.