This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Unitygain opamp with additional Vref pin with single and dual channel

Dear,

I am searching for unitygain opamp with Additional Vref pin for single and dual channel ICs.(IC operating voltage may be 3.3V or 24V would be fine else will go with the available one)

As an analog engineer would you suggest few ic's could meet these specs.

Regards,

Satya

  • Hi Satya,

    By additional Vref pin do you mean the operational-amplifier needs to have an on-board reference source? I do not find any TI operational-amplifier having on-board references. We do have a number of single and dual amplifiers that are usable over the 3.3 to 24V range and unity-gain stable for buffer applications. Do keep in mind that normally stable buffers can become unstable with capacitive loads larger than their maximum capability.

    Regards, Thomas

    PA - Linear Applicaitons Engineering