Part Number: OPA2607-Q1
Other Parts Discussed in Thread: OPA2607, OPA607, TINA-TI
Hi
I want to use OPA2607 for current sensing in sensorless motor control application.
In the datasheet, opa x607 is not unity-stable with min-gain = 6V/V. Also the Riso is needed when high load.
I do use a Rshunt = 2mΩ ,gain = 10, Riso = 56Ω,Cload = 3.3nF, PWM frequency = 15KHz
Also, I change the opa607 tina project with my design.
Seems the minus-circuit for amplifier is not as typical feedback circuit, and the simulation for phase margin is not in the plot, I can only see the degree.
Can you help me check the TINA project, see if the parameter is Ok for my application?
Below is the plot for amplitude and phase.It seems that the phase is not the phase margin para.
How can I see the phase margin for my circuit and if it match the least 45 degree safe phase margin?

below is the link for tina9 project.
/cfs-file/__key/communityserver-discussions-components-files/14/sbomb17c.tsc
Regards
Arrow