Part Number: OPA2227
Team,
my customer is comparing OPA2227U to OPA2227UA. Can you explain how to properly calculate the offset of the devices over temperature?
-
Add the temperature-dependent offset to the offset at 25°C ?
-
Add the temperature-dependent offset to the offset already given in the temperature range [-40;+85]?
How should the offset voltage in the range [-40;+85°C] be interpreted?
- Is the offset derivation already taken into account?
- Is the max offset @85°C 100µV or 0.6µV*(85-25)+100µV?
Thanks