Part Number: TLV9062
We are using the TLV9062 in a peak detector circuit. The impulse can be either positive or negative with a max impulse magnitude of +2.5V or -2.5V.
We basically have one circuit using the noninverting input for positive impulse and another circuit for the negative impulse shown below.
We have simulated the attached circuit in TINA and it works, but I am concerned with our configuration being a single voltage rail and V- tied to ground.
It seems like this should be a negative supply rail.

Thanks