Part Number: THS2630
Other Parts Discussed in Thread: OPA1633, OPA1632
I am looking for a single-ended to differential ADC driver.
The input is a single-ended signal span between -12 V & +12 V, frequency up to 25 MHz. I need to convert the +/-12 V input to a fully differential 5 V signal common-mode at +2.5 V for the ADC to sample, of cause I want to preserve the signal as much as possible in term of distortion & noise.
It appears that both THS2630 & OPA1633 (both are PREVIEW part) meet my requirement, but I couldn't figure out the price tag difference of THS2630 that is costing twice as much as OPA1633. Perhaps I missed some important parameter, or I may just stick with OPA1633.
Thanks.